Other Parts Discussed in Thread: TMS320F28388D
When I try to program the Flash on the TMDSCNCD28388D Control Card, I keep getting this error:
Error connecting to the target: (Error -2131 @ 0x0)
I can successfully load and run the program to RAM and debug with XDS100v2 Emulator on the TMDSCNCD28388D Control Card.
Bu I cannot program the Flash.
When I successfully program the RAM, I use the switch settings:
Switch S1:A with both positions ON (right)
Switch S2 with position 1 OFF (left) and position2 ON (right)
When I try to program the Flash, I use the switch settings:
Switch S1:A both position 1 and position2 OFF (left). I also tried with position 2 ON (right), but it makes no difference.
Switch S2: both position 2 and position 2 are OFF (left).
I tried cycling power and pushing reset.
Still cannot get the Flash to program. Yet, I have no problems programming and running the RAM.
How can I fix this issue?
Thanks.