This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025: Problem of CMPSS false triggering

Part Number: TMS320F280025

Dear team:

When testing cmpss module, my customer found that the protection function would be triggered by mistake when the actual voltage was only 1.9V. The protection will still be triggered after grounding the corresponding pin (pin 8).

What are the possible causes? Here is the customer code:

void InitComp(void)
{
/* set up the GPIO and X-BAR input configurations before enabling the TZ*/
EPwm1Regs.TZSEL.all = 0x0;
EPwm2Regs.TZSEL.all = 0x0;

/* Initialize Analog Subsystem */
EALLOW;
AnalogSubsysRegs.CMPHPMXSEL.bit.CMP1HPMXSEL = 1; // Bits to select one of the many sources on CopmHP inputs. Refer to Pimux diagram for details.
EDIS;

/* Initialize Comparators */
EALLOW;
//Cmpss1Regs.COMPCTL.all = 0x9414;
Cmpss1Regs.COMPCTL.bit.COMPHSOURCE = 0; // 0 High Comparator Source Select
Cmpss1Regs.COMPCTL.bit.COMPHINV = 0; // 1 High Comparator Invert Select
Cmpss1Regs.COMPCTL.bit.CTRIPHSEL = 1; // 3:2 High Comparator Trip Select
Cmpss1Regs.COMPCTL.bit.CTRIPOUTHSEL = 1; // 5:4 High Comparator Trip Output Select
Cmpss1Regs.COMPCTL.bit.ASYNCHEN = 0; // 6 High Comparator Asynchronous Path Enable
Cmpss1Regs.COMPCTL.bit.COMPLSOURCE = 0; // 8 Low Comparator Source Select
Cmpss1Regs.COMPCTL.bit.COMPLINV = 0; // 9 Low Comparator Invert Select
Cmpss1Regs.COMPCTL.bit.CTRIPLSEL = 1; // 11:10 Low Comparator Trip Select
Cmpss1Regs.COMPCTL.bit.CTRIPOUTLSEL = 1; // 13:12 Low Comparator Trip Output Select
Cmpss1Regs.COMPCTL.bit.ASYNCLEN = 0; // 14 Low Comparator Asynchronous Path Enable
Cmpss1Regs.COMPCTL.bit.COMPDACE = 1; // 15 Comparator/DAC Enable


Cmpss1Regs.DACHVALS.bit.DACVAL = 3723; // 20A / #define ADC_CURRENT_BUSIN_OC_FIXED_COEFF (0.0052882)
Cmpss1Regs.DACLVALS.bit.DACVAL = 3723; // 20A / #define ADC_CURRENT_BUSIN_OC_FIXED_COEFF (0.0052882)

//Cmpss1Regs.COMPLOCK.all = 0x000F;
Cmpss1Regs.COMPLOCK.bit.COMPCTL = 1; // 0 COMPCTL Lock
Cmpss1Regs.COMPLOCK.bit.COMPHYSCTL = 1; // 1 COMPHYSCTL Lock
Cmpss1Regs.COMPLOCK.bit.DACCTL = 1; // 2 DACCTL Lock
Cmpss1Regs.COMPLOCK.bit.CTRIP = 1; // 3 CTRIP Lock
EDIS;

/* Initialize EPwmXbarRegs */
EALLOW;
EPwmXbarRegs.TRIP4MUX0TO15CFG.bit.MUX0 = 0; // 1:0 Mux0 Configuration for TRIP4 of EPWM-XBAR
EPwmXbarRegs.TRIP4MUXENABLE.bit.MUX0 = 1; // ePWM XBAR Mux Enable for TRIP4
EPwmXbarRegs.TRIPOUTINV.bit.TRIP4 = 0; // ePWM XBAR Output Inversion Register
EDIS;

/* Initialize DC */
EALLOW;
EPwm1Regs.DCTRIPSEL.bit.DCAHCOMPSEL = DC_TRIPIN4; // 3:0 Digital Compare A High COMP Input Select
EPwm1Regs.DCTRIPSEL.bit.DCBHCOMPSEL = DC_TRIPIN4; // 11:8 Digital Compare B High COMP Input Select
EPwm1Regs.DCACTL.bit.EVT2SRCSEL = DC_EVT2; // 8 DCAEVT2 Source Signal
EPwm1Regs.DCACTL.bit.EVT2FRCSYNCSEL = DC_EVT_ASYNC; // 9 DCAEVT2 Force Sync Signal

EPwm2Regs.DCTRIPSEL.bit.DCAHCOMPSEL = DC_TRIPIN4; // 3:0 Digital Compare A High COMP Input Select
EPwm2Regs.DCTRIPSEL.bit.DCBHCOMPSEL = DC_TRIPIN4; // 11:8 Digital Compare B High COMP Input Select
EPwm2Regs.DCACTL.bit.EVT2SRCSEL = DC_EVT2; // 8 DCAEVT2 Source Signal
EPwm2Regs.DCACTL.bit.EVT2FRCSYNCSEL = DC_EVT_ASYNC; // 9 DCAEVT2 Force Sync Signal
EDIS;

/* Initialize TZ */
EALLOW;
EPwm1Regs.TZDCSEL.bit.DCAEVT2 = TZ_DCAH_HI; // 5:3 Digital Compare Output A Event 2
EPwm1Regs.TZSEL.bit.DCAEVT2 = 1; // 6 DCAEVT2 CBC select
EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // 1:0 TZ1 to TZ6 Trip Action On EPWMxA
EPwm1Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // 3:2 TZ1 to TZ6 Trip Action On EPWMxB
EPwm1Regs.TZCLR.all = 0xFFFF; // Trip Zone Clear Register

EPwm2Regs.TZDCSEL.bit.DCAEVT2 = TZ_DCAH_HI; // 5:3 Digital Compare Output A Event 2
EPwm2Regs.TZSEL.bit.DCAEVT2 = 1; // 6 DCAEVT2 CBC select
EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // 1:0 TZ1 to TZ6 Trip Action On EPWMxA
EPwm2Regs.TZCTL.bit.TZB = TZ_FORCE_LO; // 3:2 TZ1 to TZ6 Trip Action On EPWMxB
EPwm2Regs.TZCLR.all = 0xFFFF; // Trip Zone Clear Register
EDIS;

Best regards