Greetings Forum,
I'm a bit stuck debugging issue im having hence the post.
I created new PCB with a micro after studying abit the reference design files for a F28388D microcontroller from TI folder. I was not able to obtain this micro due to chip shortages.
After soldering the pcb components power, supplies decoupling caps, inductors I was expecting to have some communication with the microcontroller. Im getting error
IcePick_C_0: Error connecting to the target: (Error -183 @ 0x0) The controller has detected a cable break far-from itself. The user must connect the cable/pod to the target. (Emulation package 9.3.0.00032)
Im using a FT2232HL cheap adapter from ebay as a programmer.I can use used it with another micro (F28069M) custom PCB that I designed.
Im using a .F28388D.ccxml for a target configuration.
I checked the pins for bridges and shortages and pins correct voltages on the 3.3V and 1.2V rails.
I also tried suppling the power from the probe with no luck.
What should I check for next.
Im attaching pdf of the schematic for eagle.mcupdf.pdf