Other Parts Discussed in Thread: C2000WARE, TMDSCNCD28388D
There is example for USB used as Mass Storage Device To SD Card?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There is example for USB used as Mass Storage Device To SD Card?
Asaf,
You can refer to the "usb_ex7_host_msc" example in C2000Ware located at <C2000WareInstallDir>\driverlib\f2838x\examples\c28x\usb folder.
This example demonstrates reading a file system from a USB mass storage class device. It makes use of FatFs, a FAT file system driver. It provides a simple command console via the SCI for issuing commands to view and navigate the file system on the mass storage device.
Best Regards
Siddharth
the example should work if i connected only pins: GPIO42 - USB_N, 43 - USB_P , 46 - USB_VUSB
Hi,
The device is not recognize by the PC and Appear on Device Manager as Unknown USB Device
Hi,
Which device are you trying to connect? You may have to install the drivers for the device that you are trying to connect.
Best Regards
Siddharth
Hi,
I use MSC USB example and connect it to PC the PC is not recognize the Device?
there is example for mass storage device?
advice
Pls check if the driver needs to be installed. Are you trying this example on the Control card ?
Best Regards
Siddharth
I have not the driver for that, I search it on the SDK location folder.
I don't know what is it control card, i want to connect it to PC
Hi,
Where are you connecting the Mass Storage device? Are you using the control card TMDSCNCD28388D?
Best Regards
Siddharth
Are you able to connect to CCS using this custom board? When you connect the USB mass storage device, it should enumerate and identify the device. What is the VID and PID of the device that you are connecting?
Best Regards
Siddharth