Other Parts Discussed in Thread: TMDSEMU200-U
Issue in Configuring TMS320F28033 in UniFlash
I'm experiencing some problem on programming TMS320F28033, and the debugger is Texas Instruments XDS2xx USB Debug Probe.
In UniFlash, the error message is:
[ERROR] C28xx: Error connecting to the target: (Error -180 @ 0x0) The controller has detected a target power loss.
The user must turn-on or connect the power supply for the target. (Emulation package 9.5.0.00141).
I'm using Uniflash 7.0.0
I believe that means the TVRef pin is not seeing 3.3V. But I'm sure the 3.3V is provided to pin 5 of the debugger which is TVRef.
And it is reference to the same ground of the 3.3V to the DSP.
Any help would be appreciated! Thanks!
Kedao