Part Number: TMS320F28388D
Other Parts Discussed in Thread: ADS7883
Hi all!
I want to read ADS7883 at maximum speed so 48 MHz. Therefore, I directly wanted to use SPI peripherals in high speed mode. However, high speed spi only works on certain gpios(see the pic). Because of this restriction I have pin allocation issues now. Also, I don't know if 48 MHZ is high speed for F2838x. I couldn't see any info about it in the reference manual also.
My question is can I use SPI's at 48MHz with other GPIO's? What is the maximum SPI CLK frequency without using high speed mode?
cheers,