Hi team,
According to the datasheet, the Q version chip can work in up to 125°C ambient temperature, and the operating junction temperature can be up to 150°C. Meanwhile, there is a temperature sensor inside the package to measure the junction temperature so that the SW can do high-temperature protection based on the result of temperature sensor.
But actually, there is error and delay between actual junction temperature and the measured one. So do we have recommended threshold value for junction temperature or ambient temperature? Or do we have other methods to quickly and precisely protect the chip from burning out?
Best Regards,
Will