Part Number: TMS320F280025
Other Parts Discussed in Thread: C2000WARE
Dear team:
After transplanting the Lin module configuration code of f28034 to f280025, my customer found that the chip could not receive data. Is there anything to pay attention to in the Lin configuration of these two chips?
The following is the code for f280025:
EALLOW;
CpuSysRegs.PCLKCR19.bit.LIN_A = 1;
GpioCtrlRegs.GPAPUD.bit.GPIO28 = 0; //GPIO28 (LIN TX)
GpioCtrlRegs.GPAPUD.bit.GPIO29 = 0; //GPIO29 (LIN RX)
GpioCtrlRegs.GPAQSEL2.bit.GPIO29 = 3;
GpioCtrlRegs.GPAQSEL2.bit.GPIO29 = 0x01;
GpioCtrlRegs.GPACTRL.bit.QUALPRD3 = 0x03;
GpioCtrlRegs.GPAGMUX2.bit.GPIO28 = 2;
GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 2;
GpioCtrlRegs.GPAGMUX2.bit.GPIO29 = 2;
GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 2;
EDIS;
//Lin register configuration
EALLOW;
LinaRegs.SCIGCR0.bit.RESET = 0;
LinaRegs.SCIGCR0.bit.RESET = 1;
LinaRegs.SCIGCR1.bit.SWnRST = 0;
LinaRegs.SCIPIO0.bit.RXFUNC = 1; //These two sentences are not available on 28034.
LinaRegs.SCIPIO0.bit.TXFUNC = 1; //Other configurations are the same as 28034.
LinaRegs.SCIGCR1.bit.SLEEP = 0;
LinaRegs.SCIFLR.bit.TXWAKE = 0;
LinaRegs.SCIFLR.bit.TXEMPTY = 1;
LinaRegs.SCIFLR.bit.TXRDY = 1;
//Configure for data reception
LinaRegs.SCIGCR1.bit.RXENA = 1;
LinaRegs.SCIGCR1.bit.TXENA = 0;
LinaRegs.SCIGCR1.bit.TIMINGMODE = 1; //Asynchronous Timing
LinaRegs.SCIGCR1.bit.CLK_MASTER = 1; //Enable SCI Clock
LinaRegs.SCIGCR1.bit.CONT = 1; //Continue on Suspend
LinaRegs.SCISETINT.bit.SETRXINT = 1;
LinaRegs.SCISETINT.bit.SETTXINT = 1;
LinaRegs.SCIFORMAT.bit.CHAR = 0x7;
LinaRegs.SCIGCR1.bit.SWnRST = 1;
EDIS;
LinaRegs.SCIPIO0.bit.RXFUNC = 1;
LinaRegs.SCIPIO0.bit.TXFUNC = 1;
These two codes are not available on 28034. Other configurations are the same as 28034.
In addition, the above configuration method can only view the register configuration in registers. I don't know how to view the register configuration in expressions?
Best regards