This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: TIDM-DC-DC-BUCK- DC-DC Synchronous Buck converter reference design with F28377S

Part Number: TMS320F28377S
Other Parts Discussed in Thread: SFRA, TIDM-1000

Dear Experts, 

Looking at the Resource Explorer, the example project for TIDM-DC-DC-BUCK- DC-DC Synchronous Buck converter is only available for F28004X family.  

Is there an example project for a Buck converter with SFRA for F2837x? 

If not, is there a migration guide available to use this example with F28377S, instead of F28004x ? 

I could only find migration guides between F2837x to F2838x and F28004x to F28002x ...

Thanks and best regards,

Gregor

  • Hi Gregor,

    There is no Buck converter example on F2837x device. The reason you only  see migration guide between F2837x to F2838x and F28004x to F28002x is because they are considered as same class of device (with similar clock frequency and memory capability). There is no migration guide from F28004x to F2837x device.

    Since the example project is written in driverlib, it should be relatively easy to do the migration. You may refer to TIDM-1000, since it is the only example program that we supports both F28004x and F2837x (F28379D) devices.

    Let me know if you have other specific questions.

    Han