Dear Champs,
I am asking this for a customer.
The user wants to use 48-pin F280033SPT, but because sample availability, they can only use superset F280037CSPT.
Therefore, they are asking if they can develop codes on F280037CSPT and then 100% same as that for F280033SPT when F280033SPT is available?
In my understanding,
1. They should avoid use part ID.
2. They should avoid using any peripherals that F280033SPT does not have.
3. They should use the .cmd file for F280033SPT.
However, I don't see the specific F280033SPT .cmd in the latest CCS11.1 folder C:\TI\ccs1110\ccs\ccs_base\c2000\include.
Would you please help specify where it is?
4. Is there anything else the user has to be aware in order to use the same codes from superset F280037CSPT to F280033SPT?
Wayne Huang