The TMS320F28027 program cannot be loaded with the following error:
(See the captured image below)
The error code is as follows.
----- -----
C28xx: Flash Programmer: Device is locked or not connected. Operation canceled.
C28xx: File Loader: Memory write failed: Unknown error
C28xx: GEL: File: F2802x_FLASH \ PHASE3.out: Load failed.
----- -----
The TMS320F28027 will not recover even if the power is turned off or the CCS is restarted. Also, you cannot load the OUT file of another project.
I suspect that the CSM has been locked for some reason. It's okay for the internal code to disappear completely, so is there a way to get it back?
Thanks,
Koki