This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: What type of LCD display could be interfaced with TMS320F28335 to display different parameters of a motor

Part Number: TMS320F28335


Hi Members,

I am working to implement a Faulty motor experimental setup, where inter-terns faults would be created and different motor parameters like speed, fault type and fault location would be displayed on LCD or LCDs. Please can any one suggest me which type of LCDs can be interfaced with TMS320F28335. If possible then please tell me what Pins of the DSP would be used and how many Pins would be used. Does TMS320F28335 will be compatible with a LCD display. Or please suggest suitable LCD display(s) for TMS320F28335. 

Sincerely 

Shamsher