Other Parts Discussed in Thread: POWERSUITE, C2000WARE
I have CCS 11 installed. Path on my disk is "C:\ti\ccs1110"
I also installed DigitalPowerDSK (along with powerSUITE). Path on my disk is "C:\ti\c2000\C2000Ware_DigitalPower_SDK_4_00_00_00".
I am trying to follow a design guide that want me to import projects from the DigitalPowerSDK and open powerSUITE projects, etc. At every turn I get either direct or indirect indication that CCS can't see the installed SDK. Maybe because it's in the wrong folder location on my machine?
Can anyone help me get CCS to "see" the installed DigitalPowerSDK? How can I check? Can I point CCS to the location? Do I need to re-install the SDK to a special location (when I installed it, I just use the recommended default location of "C:\ti\c2000\C2000Ware_DigitalPower_SDK_4_00_00_00".
Thank you.