Other Parts Discussed in Thread: CONTROLSUITE
Hello, I have designed in the components from the CC2803x and DRV8312EVM into my project with the exception that I am using my host microcontroller as the Windows "GUI" interface to the C28035 over UART. I notice that the communication protocol is mostly hidden in a library file in the code project, which makes porting the code to my host difficult. Instead of having to reverse engineer the protocol via logic analyzer, would you please share the comm protocol with me? I would just like the ability to duplicate the commands from the Windows GUI onto my host and nothing more to control a BLDC motor.
Thanks!