Part Number: TIDM-02010
Hi
There are issues still in BUILD 3 AND build 4 of Compressor Motor
1. BUILD 3 - NO Load motor running fine . Tested upto 3000rpm
2. BUILD 3 - WIth Load - Motor running upto 28Hz (speed), upfront 30Hz the motor stops. There is no fault. The shaft is not rotating but there is some vibration inside the motor.
3. BUILD 4 - MOTOR running with CRANKY noise, This issue is not getting resolved.
Pls revert with a possible solution asap