Because of the Thanksgiving holiday in the U.S., TI E2E design support forum responses may be delayed the week of Nov. 21. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28020: Datasheet spec's 40MHz, but measures 50MHz?

Part Number: TMS320F28020
Other Parts Discussed in Thread: C2000WARE, TMS320F28027

Hi All,

The math to set up I2C and SCI clock rates hasn't been working quite right.  When I select a value, the data rates are a little higher than anticipated.  I just want to make sure I understand correctly.

The datasheet (SPRS523P rev Feb 2021) for TMS320F28020DAT shows that this particular part is 40MHz (see 28020 column of Table 6-1).

When I enable XCLKOUT on GPIO18, I see 50MHz on the scope, with SYSCTRL::XCLK set to 2 (div by 1).  With it set to 0 (div by 4), I get 12.5MHz.

Here's an image of the shipping label:

Can you help me understand this?

Thanks,
robin

  • Robin,

    Even though the device is only guaranteed to work up to 40MHz, there is nothing that prevents you from using a PLLCR value that exceeds this.  I think that you may be running an example that was has the PLLCR value for another device in this family(F28022 I think) that is spec'd at 50MHz.

    For 40MHz, assuming you are using the internal oscillator(10MHz), you need to change the PLLCR value to 4(from 5). 

    If this is happening from a C2000Ware example that is built for this specific device, please let me know so we can file a bug against this example

    Best,

    Matthew

  • Of course (face palm)!

    It's been a while since I started this project, and I don't remember all the details, but it probably started life as example code on the LaucnXL-F2802x, which is running a TMS320F28027 probably at 60MHz.  I'm not sure how I got to 50MHz, but your comment about PLLCR is spot on.

    Thanks for your help.