Other Parts Discussed in Thread: MOTORWARE
Hi,
I am testing the DRV8301-69M-KIT drive kit with simply the demonstration GUI (instaspin-motion). I don't have a lot of experience with microcontrollers and c projects so this is easier for me. On the "Motor Identification" tab, I can choose the "user.h settings" for the identification method. If I click on "Identify Motor", I see some user.h default settings appearing. My question is: How can I change the user.h default settings so that I can skip the identification process? Where is the user.h file used for the demonstration GUI?
During my dynamometer tests due to some faults which I cannot reset (using the "Reset DRV fault" button in the GUI). I have to shut down the drive and do the identification step each time which is time consuming.
Thank you
Jeff