Other Parts Discussed in Thread: POWERSUITE, SYSCONFIG
hi,
How can I change TIDM-1022 to CCM + single phase(not interleave)?
BR,
frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
How can I change TIDM-1022 to CCM + single phase(not interleave)?
BR,
frank
Hi Frank,
I think you use powerSUITE to choose enable interleaved and that will be CCM. If you select single phase and it will be automatically enable valley switching for DCM mode.
So in order to do CCM + single phase you have to manually change the code using the non-powersuite version in SDK.
Regards,
Chen
Chen,
Not sure if I understand correctly. Please correct me if I am wrong.
-import TIDM-1022 project and use sysconfig to select "Single Phase PFC".
- add code below.
valley_switching_MODE = valley_switching_disable;
is that correct?
BR,
frank
Hi Frank,
I feel it might need some additional code updates other than
valley_switching_MODE = valley_switching_disable;
For example, to double confirm the PWM settings.
customer may need to go through the code a little bit to validate it.
Regards,
Chen