Hello,
I have a question on the Design Guide TIDM-1000 of Vienna Rectifier-Based, Three-Phase Power Factor Correction (PFC) Reference Design Using C2000 MCU.
Specifically it is on the output voltage specification.
TIDM-1000 outputs 700VDC nominal for the three-phase input of 400 VL-L, and the 650V power MOSFET of IPP65R190C7FKSA1 is used as the switching device.
We are planning to develop a Vienna Rectifier which has the output voltage of 1000V.
I am wondering if I can use the hardware of TIDM-1000 basically for this purpose.
Apparently the DC-link capacitors may have to upgraded for the DC-link voltage of 1000V.
In other words, my question is whether the 650V power MOSFET of IPP65R190C7FKSA1 can be still used as the switching device when the DC-link voltage is increased to 1000V.
Thank you for your advice.
With regards,
JS Yoo