This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MOTORWARE: Migration "Instaspin Motion Software" Between F28069M and F280039C

Part Number: MOTORWARE
Other Parts Discussed in Thread: TMDSHVMTRINSPIN, HVPMSMMTR, TMDSCNCD280039C, DESIGNDRIVE

Dear Experts,


I am using Motorware's instaspin lab 13c to evaluate driving HVPMSMMTR with TMDSHVMTRINSPIN. DSP is F28069M.
I was able to check the operation in debug mode using the on-board debugger of F28069M board.

①Now let me ask the title question. My next goal is to achieve the above lab13c operation with F280039C.
 However, I confirmed that F280039C only supports InstaSPIN-FOC for PMSM, doesn't support InstaSPIN-Motion. 
 In other words, even if I could adapt the Lab13c program to the F280039C pinout and migrate it perfectly, wouldn't it work? Or is it possible that it works?

In addition, I have two related questions.
②Has sample code for achieving sensored position control or sensored speed control for the F280039C been released?
③Are there any future plans to support Instaspin Motion with the F280039C?

Thank you.