Other Parts Discussed in Thread: C2000WARE, TIDM-02009
Hi team,
Here's an issue from the customer may need your help:
The customers are developing an automotive primary drive motor drive with plans to use the C2000 series as the master chip. The models currently under consideration are F28335-Q1, F28379D-Q1, F280049-Q1, and F28386D-Q1.
They have previously worked on projects on the F28335 and have development experience on the third generation C200 and have referenced to following two documents to meet the needs of ASIL-D:
The customer has the following questions:
1) Is functional safety support libraries all in C2000WARE? Or is it required an additional request? Or are there export controls?
2) Since customer are more familiar with the F28335, is it appropriate to develop on the F28335-Q1? For functional safety, does the F28335 also have the same software support as the third generation C2000?
3) Is there a reference design? They've noticed TIDM-02009, but it does not seem to have functional safety in the source code.
4) Does TI have support for autosar and auto code generation?
Could you help check this case? Thanks.
Best Regards,
Cherry