Hi
I have a F280049 project file (.projectspec), all files are linked to the original folder.
What's the normal way to specify a search path to those library files and link files (.cmd)?
I don't want to use "-I" to specify an absolute path to the original folder in the project file.
The project is as the followings:
<projectSpec> <project name="1_ph_Pwm_with_DC_input" device="TMS320F280049M" cgtVersion="16.9.1.LTS" launchWizard="False" linkerCommandFile="" > <configuration name="1_RamDebug" compilerBuildOptions="--opt_level=off -v28 -ml -mt --cla_support=cla2 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu0 --define=CPU1 --diag_warning=225 --diag_suppress=10063 --display_error_number" linkerBuildOptions="--stack_size=0x30A -heap=0 --entry_point code_start" /> <configuration name="2_RamRelease" compilerBuildOptions="--opt_level=3 -v28 -ml -mt --cla_support=cla2 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu0 --define=CPU1 --diag_warning=225 --diag_suppress=10063 --display_error_number" linkerBuildOptions="--stack_size=0x30A -heap=0 --entry_point code_start" /> <configuration name="3_FlashRelease" compilerBuildOptions="--opt_level=3 -v28 -ml -mt --cla_support=cla2 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu0 --define=CPU1 --define=_FLASH --diag_warning=225 --diag_suppress=10063 --display_error_number" linkerBuildOptions="--stack_size=0x30A -heap=0 --entry_point code_start" /> <configuration name="4_FlashRamRelease" compilerBuildOptions="--opt_level=3 -v28 -ml -mt --cla_support=cla2 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu0 --define=CPU1 --define=_FLASH --diag_warning=225 --diag_suppress=10063 --display_error_number" linkerBuildOptions="--stack_size=0x30A -heap=0 --entry_point code_start" /> <file action="link" path="1_ph_Pwm_with_DC_input.c" targetDirectory="" /> <file action="link" path="F28004xCla.cla" targetDirectory="" /> <file action="link" path="PsBiosRamF004xFloat.lib" targetDirectory="" applicableConfigurations="1_RamDebug,2_RamRelease" /> <file action="link" path="PsBiosRomF004xFloat.lib" targetDirectory="" applicableConfigurations="3_FlashRelease,4_FlashRamRelease" /> <file action="link" path="cla2_math_library_datarom_fpu32.lib" targetDirectory="" /> <file action="link" path="F28004x_CLADATROM_Symbols_fpu32.lib" targetDirectory="" /> <file action="link" path="f28004x_headers_nonbios.cmd" targetDirectory="" /> <file action="link" path="F280049_RAM_lnk.cmd" targetDirectory="" applicableConfigurations="1_RamDebug,2_RamRelease" /> <file action="link" path="F280049_FLASH_lnk.cmd" targetDirectory="" applicableConfigurations="3_FlashRelease" /> <file action="link" path="F280049_FLASH_RAM_lnk.cmd" targetDirectory="" applicableConfigurations="4_FlashRamRelease" /> </project> </projectSpec>
Thanks,
Jiakai