This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSECATCNCD379D: is this same as TMDSDOCK28379D + ethernet card

Part Number: TMDSECATCNCD379D

Hello,

I do not want to use ethernet card. TMDSDOCK28379D is unavailable, hence planning to buy this.

1) WIll the same code developed for TMDSDOCK28379D work with this product?

2) I see that docking station is not included along with this item. Can the docking station of TMDSDOCK28379D be used along with TMDSECATCNCD379D?

Regards,

  • Hi Shyam,

    1) WIll the same code developed for TMDSDOCK28379D work with this product?

    Yes. The controlCARD is same. So all the codes developed for TMDSDOCK28379D will work.

    I see that docking station is not included along with this item. Can the docking station of TMDSDOCK28379D be used along with TMDSECATCNCD379D?

    Yes. It does not come with docking station. If you already have docking station, then it should work.

    Thanks & Regards,

    Santosh