Hello,
We are building custom board using TMS320F28377SZWTQ. It is a mother-daughter board design. TMS320F28377S is on the daughter board that seats on the motherboard. JTAG is on the motherboard. Distance between TMS320F28377S JTAG pins and port is about 5 inches. We are going to use XDS-110 for CCS connection and using 20 pin connector. Can you please verify the attach JTAG port circuit and connections, is there any changes required for proper TMS320F28377S JTAG connection?
Regards,
Sid