This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO3: dis6x segmentation fault

Part Number: CCSTUDIO3

I get this error when trying to use dis6x. Perhaps it is because we use CCS Version: 11.1.0.00011 or maybe because dis6x is only ccs1040 and is not meant for later versions.

c:\work\tools>dis6x C:\work\flash_kernel_c28x_dual_ex1_c28x1\CPU1_RAM\f2838x_codestartbranch_cpu1.obj

Disassembly of C:\work\flash_kernel_c28x_dual_ex1_c28x1\CPU1_RAM\f2838x_codestartbranch_cpu1.obj:

INTERNAL ERROR: dis6x experienced a segmentation fault

This is caused by a defect in the TI Disassembler.
TI Customer Support may be able to suggest a workaround to avoid this.

Upgrading to the newest version of the compiler may fix this problem.

Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler".  See the link titled
"Submitting an issue".

We need to see this ENTIRE error message and a complete, reproducible
test case including ALL of the command-line options.

Thanks,

John