Hi,
One of my projects had a high requirement for the number of PWM outputs, which required 48 PWM outputs (complementary with dead zone). But 28388 only has 32 PWM outputs. So I came up with the idea of using 28388 CLB to generate part of the PWM output. However, due to the limited resources of CLB, I can only use the 8 modules of CLB and 8 ePWM modules to generate 32 PWM outputs( using ePWM1A and ePWM1B combined with CLB1 to generate 4-channel PWM output), so I use the DB module of ePWM to generate complementary deadband PWM outputs to meet the remaining output requirements.
I see that the clock of CLB is synchronized with the clock of PWM in TRM, but I still want to ask, could the PWM generated by these two methods be considered to be completely equivalent?
Thanks&Regards,
Zhu