This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28069MISO: Compiler error return c++ source files are not allowed for CLA

Part Number: TMDSCNCD28069MISO

Hi, 

I am currently using compiler TI v22.6.0.LTS and when I am trying to compile my project (composed of .cpp .c files) with the option ''Treat C files as CLA files'' check I get the following error message with from all my .cpp files:
C++ source files are not allowed for CLA

I get the same error when using TI v21.6.1.LTS. 

However, on a older project TI v18.12.0.LTS was used and there was no error. I tried for this project and same result.

I would prefer to use a more recent compiler if possible.

Thanks!

Etienne