I am currently trying to connect to the control card mentioned above via a USB connection without a docking station. When attempting to use CCS to connect to my board I am given the error "2131 - Unable to access device register.". I have tried restarting the board and ensured that the probe being used is correct however the problem still persists. Is it possible to run code on this card with just a USB connection or do I require the docking station?