Hi,
I need some tips on how to maximize the start torque when using InstaSPIN FOC+MOTION together with a low-inductance sensorless motor. I have read through chapter 14 in the instaspin user guide, and have enabled all recommended features (rs recalibration, rs online, forced angle). However, I want to know how to tune it even more. I have a use-case where I have very high static friction I need to overcome. Here are some questions I have:
- Is there any recommended way to tune the force angle open loop control for a particular motor (by setting zero_speed_limit and forced_angle_frequency)?
- The MOTION software is tuned with only one variable (system bandwidth). Would it be possible to get better performance by switching to using the PI controller that comes with FOC?
- How important is the SW limit for max current (USER_MOTOR_MAX_CURRENT)? I know this is only a SW limit and is not really limiting the motor from drawing more current. However, would an increase in this variable typically lead to higher start torque?
Also, if you have any other tips or relevant questions I would love to hear them!
Best regards,
Jørgen