Hi,
I am using the TMDSDOCK28379D for an application, and i dont need to use the pin from 121 to 180.
Also, i don't have the docking on my board for those pin (121 to 180)....
Is the card going to work well without de 5V and GND on the pin requiring it between 121 and 180?
Thanks for the support!
Vincent Beaulieu-Gagnon