Other Parts Discussed in Thread: C2000WARE
Is there an example GEL file that configures the EMIF for the TMS320F28377S, preferably for an SRAM? If not, something close would be helpful.
Thanks in advance,
Paul Hetherington
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there an example GEL file that configures the EMIF for the TMS320F28377S, preferably for an SRAM? If not, something close would be helpful.
Thanks in advance,
Paul Hetherington
Paul,
There are examples available in C2000ware which demonstrate how to configure EMIF for the device specified above.
They can be accessed at the following location:
C2000Ware_X_XX_00_00\driverlib\f2837xd\examples\cpu1\emif
Thanks.
Hi Sahil,
I don't see a gel file in the folder you provided.
Im looking for an example gel file for the 28377 EMIF. Or something close that could be used as a starting point.
At the moment Im using the TI Launchpad LAUNCHXL-F28279D with the EMIF Daughter Card reference design plugged in. My goal is to download to and run code from the Daughter Cards SRAM using Code Composer.
Thanks,
Paul Hetherington
Paul,
I am checking with the team and will get back to you on this soon.
Thanks.
Paul,
There is no GEL file that you are asking for. The examples as mentioned above is all the support we have for now.
Thanks.