This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28379D: TMDSCNCD28379D - USB bootloader - Enumerating Failure

Part Number: TMDSCNCD28379D
Other Parts Discussed in Thread: C2000WARE

Hello,

I am trying to get the USB bootloader example working - C:\ti\c2000\C2000Ware_4_03_00_00\utilities\flash_programmers\usb_flash_programmer. I have read through some of the other post but did not see a solution.

Here are my steps.

  1. Launched CC with a project
  2. Selected CPU reset within CC
  3. Went to 0x0D00 memory location
  4. Set 0x0D00 to 0x0C5A and start project
  5. Right clicked on F28x7x_USB_Boot_Loader.inf in C:\ti\c2000\C2000Ware_4_03_00_00\utilities\flash_programmers\usb_flash_programmer\windows_driver to install the device driver
  6. Plugged in MCU control board USB Host Controller J8 to computer I installed device driver
  7. Typed the following usb_flash_programmer.exe -l at a prompt at C:\ti\c2000\C2000Ware_4_03_00_00\utilities\flash_programmers\usb_flash_programmer
  8. I then get the following output

Here is showing setting 0X0D00 to 0x0C5A

Here is looking at the device when I plug it in:

Note: I have also run the usb_ex7_host_msc.c and usb_ex4_dev_bulk.c successfully and installed the appropriate device driver in the bulk example instance.

Any insight as to what I am doing wrong would be greatly appreciated.