Other Parts Discussed in Thread: TMDSCNCD28069, CONTROLSUITE, TMDSCNCD28035ISO, DRV8301
Install the TMDSCNCD28069 ISO control card
I'm trying to activate the DRV8301-69-KIT EVM board. Operates the Level1 example code for C:\ti\controlSUITE\development_kits\DRV830x-HC-C2-KIT_v105\PM_Sensorless, which works well up to the pole voltage command. However, the PWM waveform does not output and the motor does not drive as a result. Following the controlsuite docs manual does not resolve it. Also, replacing it with TMDSCNCD28035ISO control card still does not solve it.
However, when the TMDSCNCD28069MISO control card is installed and driven via InstaSpin-Motion, it will function normally.
Does anyone have the same problem as me?