This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-HV-1PH-DCAC: Change to 800-V DC input, 110-V AC output

Part Number: TIDM-HV-1PH-DCAC

Hi team,

If the customer want to change to 800-V DC input, 110-V AC output, is it only required to change the tolerance values of capacitors, IGBTs, etc.? Or is it also required to add an additional DCDC buck to 380V in the circuit? 
Could you help check this case? Thanks.
Best Regards,
Cherry