Other Parts Discussed in Thread: C2000WARE,
I have an issue in figuring out the corresponding physical pins on TMDSHSECDOCK-rev F dock station for a code generated from PSIM Simcoder. In the hardware configuration window in PSIM (as shown below in the screenshot), A3 is configured as ADC In. However I couldn't find the corresponding pin in the dockstation because in the 180_HSEC8_DV_pinout_Rev_F file, there is no such A3, also there is no ADC3!
I have also the same issue in the GPIO pins where in PSIM F28004x configuration I have GPIO0, GPIO1, GPIO2, GPIO3 configured as PWM (also attached screenshot below), still I couldn't know where are GPIO0, GPIO1, GPIO2, GPIO3 on the dockstation because the digital pins are not numbered in the 180_HSEC8_DV_pinout_Rev_F file.
My questions are:
- Is there any other pinout mapping file that I can check?
- How to match the configuration of pins in PSIM simcoder to that of the docking station TMDSHSECDOCK-rev F?