Other Parts Discussed in Thread: TMDSEMU560V2STM-U
Hi Experts,
Good day
I'm trying to program a card (TMS320F28335 Custom Board) and I get the following message:
Failed to connect to the destination:
(Error -183 @ 0x0)
The controller has detected a cable breakaway from itself.
The user must connect the cable/pod to the target.
(Emulation package 5.1.402.0)
The loader is the USB560v2 (TMDSEMU560V2STM-U) system trace. Yesterday we programmed two cards without problems and they are working, but today it gives us this error message.
I have done the indicated tests and troubleshooting (Debugging JTAG (ti.com)), but the error continues to appear. the cable is as if it were disconnected inside the equipment
Please advise
Regards,
Josel