Hello Team,
We are working on a off-grid based project. To start of with we have chosen this ref design.
1.Is there any specific reason why the voltage was only fixed at 12V to 400V conversion? In case if I shift to 48V can go to higher voltages like 600V or 800V?
2.The power output of the design is 300W. In case If I wish to scale up to 5KW or 10KW what should be done? If it cannot be done can we know the reason behind that?
3.In majority of the bidirectional DC-DC Converter designs the voltage difference between the input and the output is around 100V to 250V. Is there any specific reason for the difference in the voltage?
ex : https://www.ti.com/tool/TIDM-02002
4.How do we decide the DC Input voltage for the 1-Phase and 3-Phave Inverter? Is there any document that helps us to calculate the DC Voltage that required/mandatory for the Inverter to deliver the desired output voltage of 230V(in case of 1 phase) and 415V (in case of 3 Phase)?
It would be very kind if you can help us to clarify these queries. We appreciate your time and efforts. Thanks .