Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE
Hi,
I'm trying to debug my project without download but with active CSM key.
I set "Load symbols only" in the debug configuration and I also set the CSM key in the Flash settings.
When I debug with download everything is working as expected, but as soon as I try to debug without download I just see that "no symbols are defined" and I get the message "C28xx: Can't Run Target CPU: (Error -1041 @ 0x33A644) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.10.0.00080)".
When I disable the CSM key by setting the keys to 0xFFFF (in the file DSP2833x_CSMPasswords.asm) I'm able to debug without download.
I assumption is that I get the message since the unlock is only done before I download the project to the target, but when I just connect to the target without download the unlock is not done.
Is there any possibility to debug my project without download but a set CSM key?
Thanks in advance
Jeronimo