Part Number: TMDXIDDK379D
Other Parts Discussed in Thread: DESIGNDRIVE, TMDSCNCD28388D
Hi,
Yesterday arrived a Tecnotion UM3-N (PMSM linear motor) and I went and tried to follow the EtherCAT-Based Connected Servo Drive Using Fast Current Loop on PMSM. All went fine during Incremental Build Level 1 but when I tried the Incremental Build Level 2 and pressed run motor the TMDXIDDK379D showed some sparks next to the mains connector and the outlet power was cut off. When I tried to power it on, it happened again.
The only change that I made to the original project was changing the current limit from 8A to 0,5A so that my motor won't overheat during the tests (I didn't change any of the motor parameters for the first test but I was going to change them for the next tests). The encoder I have is a Renishaw Resolute 36bit BISS-C.
My current configuration is all power coming from mains as the DesignDRIVE IDDK User's Guide says.
The fuse is ok.
If I unplug the red cable that connects BS1 and BS2, the board powers up again. And I can connect to the board.
I've tested the voltages of M8 and M2 and they're fine, I've also tested voltages of M3 and M9 and they're also ok.
If there's anything else I could check to see if it can be fixed that would be perfect.