This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28069M: Controlling Four Motors Simultaneously

Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: BOOSTXL-DRV8301, C2000WARE

Hello E2E community,

I have a setup consisting of a LAUNCHXL-F28069M and 2 BOOSTXL-DRV8301, allowing me to control two motors simultaneously. Now, I want to extend my setup to control four motors at the same time. My understanding is that I might need 2 LAUNCHXL-F28069M and 4 BOOSTXL-DRV8301. Am I correct in this assumption?

I am aware that an alternative approach would be to use a single board (LAUNCHXL-F28069M) with 4 Electronic Speed Controllers (ESCs), but I prefer the configuration with 2 boards and 4 drivers. My main question is, if I opt for the dual-board setup, how can I effectively control both boards simultaneously?

Any guidance or insights into configuring and synchronizing two LAUNCHXL-F28069M boards with 4 BOOSTXL-DRV8301 drivers for simultaneous motor control would be greatly appreciated.

Thank you!