This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1000: information about TIDM-1000

Part Number: TIDM-1000

Hi Team,

I'm asking for my customer:

Does the input current of the Vienna rectifier vary depending on the load? What is the current range in a rectifier bridge? Can the peak current reach 10A? What is the current range on the DC side of the output?

Best Regards,

Ben

  • Hi Ben, 

    Does the input current of the Vienna rectifier vary depending on the load? - Yes. example, If adding an inductive load component will also impact the current waveforms.

    Current range is mentioned in the design guide:

    for the 10A peak. as per design guide it looks possible, whereas the sensing circuit can sense upto 12A. (refer calulation.xlsx sheet in hardware folder)

    BR,

    Uttam Reddy