This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: facing some compiler error

Part Number: TMS320F28379D

hello

If I use Compiler18.12.7 LTS compiler I'm facing error:


>> Compilation failure
source/device/subdir_rules.mk:9: recipe for target 'source/device/F2837xD_Adc.obj' failed

INTERNAL ERROR: C:\Users\akash.ahirwar\Downloads\ti-cgt-c2000_18.12.7.LTS\bin\ac2000.exe experienced a segmentation fault
while processing function (unknown or file scope) file (unknown) line 0

This is caused by a defect in the TI C/C++ Parser.
TI Customer Support may be able to suggest a workaround to avoid this.

Upgrading to the newest version of the compiler may fix this problem.

Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue".

We need to see this ENTIRE error message and a complete, reproducible
test case including ALL of the command-line options.
Include the .pp file created by option --preproc_with_comment

gmake: *** [source/device/F2837xD_Adc.obj] Error 1

If i use 22.6.2LTS compiler I'm not facing any error.

i need solution for this compiler error.

 Thank you