The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379S: TMS320F28379SZWTT

Part Number: TMS320F28379S

Hi, I have a design using the TMS320F28379SZWTT device and the s/w is done in Matlab/Simulink.

Hopefully a simple question! I have one o/p GPIO16 that is outputting a 500Hz square wave, but in my model I have GPIO16 connected to a constant block, which I can change between 0 & 1 but this makes no difference and it always o/ps the square wave. The h/w settings for the GPIO port look correct and are the same as all the other GPIO o/ps that are working correctly.

Is there a way to see if anything else is using this GPIO?

Thanks

Ian