This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-HV-1PH-DCAC: TIDM-HV-1PH-DCAC

Part Number: TIDM-HV-1PH-DCAC

Tool/software:

Hi,

I am looking at TIDM-HV-1PH-DCAC PCB and it seems that the pinout of J2,J3 connectors is in the opposite direction from the datasheet.

I would like you to look at the connectors and return to me with an answer.

Thanks,

Shlomi.

  • Sorry I meant J15,J16 connectors.

    Can you check this ,please?

    Thanks.

  • Hello Shlomo

    I should not be in the opposite direction as I have run this board multiple times and it worked. I would request you to see it again.

    Thank you

    Amir Hussain

  • Hi Amir,

    Thank you for your reply.

    I meant opposite direction according to datasheet of the connector.

    You can also see at the model of the connector where pin number one is (bottom left) while in your schematic it is pin 120.

    You can also see that the left side (where pin number 1 is located) of the connector has 64 pins and right side has 56 pins exactly the opposite from TI card.  

    Connector PN:

    HSEC8-160-01-L-DV-A-BL

    r

    I would like you to look at the connectors and return to me with an answer.

    Thanks.

  • Hello Shlomo

    I do not have the board with me this time to check it. Is this stopping you from working on the board?

    I am sure the control card can be inserted to the main board only one way and that is the correct way. So you can go ahead the connect the control card and start working on the board.

    Thanks

    Amir