Tool/software:
Hi Champ,
From the datasheet, when use internal VREG, the Cvdd total should 10-26.8uF.
How to understand the maximum 26.8uF value limitation ?
If over 26.8uF, what is the failure mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Champ,
From the datasheet, when use internal VREG, the Cvdd total should 10-26.8uF.
How to understand the maximum 26.8uF value limitation ?
If over 26.8uF, what is the failure mode?
Hi Huihuang
Please see our hardware design guide section 3.4.1 Power Requirements for context on decoupling capacitors: https://www.ti.com/lit/an/spracz9a/spracz9a.pdf.
Best Regards,
Allison
Hi Allison,
I don't think you answered my question!
You didn't provide the failure mode over 26.8uF case.
If you are not right person, please help involve the expert on this question!
Thanks!
Hi Huihuang,
The point of having the decoupling capacitance is to help control/smooth voltage spikes/drops in the power supply. But if you are using a higher capacitance, the rise time of the LDO may be slower. This could, for example, affect the device upon reset depending on the timing of when XRSn is released, so the result could put the device out of spec. The datasheet PMM section has more details on the power on timings and diagrams of the ramp ups.
Best Regards,
Allison
Hi Allison,
Could you more specific which timing will be affect?
Please list all the timing which will be affect by over 26.8uF case.
Thanks!
Hi Huihuang,
Allison is currently out of office until Tuesday 7/9 so please expect some delay in her response.
Best Regards,
Delaney
Huihuang,
As we increase the capacitance on the VDD supply we will also increase the time it takes for the internal LDO to fully ramp the 1.2V supply when it turns on. The values in the DS are derived with this in mind, in relation to when the internal POR/BOR gets released based on the VDDIO supply level. If this value is too large there may be risk that XRSn is released before the 1.2V is within the DS tolerance for this supply rail.
If customer has already placed a larger capacitance on the VDD net, they could look at the level on a scope along with VDDIO/XRSn during power up to see if there is any risk to the above occurring.
Best,
Matthew
Matt,
Can you advise which value in the DS will be affect if increase the capacitance on the VDD?
From the datasheet , i just see tw(RSL1) be related to reset, but this timing is after VDD stable not VDDIO.
Huihuang,
According to the DS, the POR on VDD will release at ~1V, and then supply will have 100us to reach spec minimum of 1.14V, so extra 140mV. Cap values published in the DS will ensure that above is met. If customer has larger cap values there may be some risk of not being at 1.14V when XRSn releases and device running out of specification.
Best,
Matthew