This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M36P63C2: I wonder if some of the GPIOs have restarted?

Part Number: F28M36P63C2

Tool/software:

hello,

We have a device that uses F28M36P63C2, we use the C2000 core to drive a motor, and the M3 core to do the external display and control. Once the customer reported that the indicator light of the equipment (M3 core, IO port direct drive, current of about 6mA) suddenly went out, and returned to normal after more than ten seconds, and the motor continued to rotate during the time when the light went out.
We checked the data that was written to flash at regular intervals through the M3 kernel and found no abnormal data.
I would like to ask, is there a possible reason that causes part of the M3 kernel to reboot? If so, what will be the reboot time? If not, I would like to know what could be causing the situation I am talking about?

thanks.