Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
I am trying to implement a multi-level converter using the F28379D development kit.
On the webpage, it says PWM (Ch) 24, but in the schematics, I see only PWM8 (schematics in attachment)
Where are the other PWM outputs located?
Are they all High Resolution PWMs (HRPWM)? I am thinking of using SiC MOSFETs and 30–50 kHz switching frequency. I remember reading somewhere that only 16 are HRPWM. Will the other PWM outputs be able to support a 50 kHz switching frequency?
Regards, MB
Edit:
A TMS320F2837xD Dual-Core Real-Time Microcontrollers Technical Reference Manual, section 15.14, page 1995 says: "typical low-frequency PWM operation (below 250kHz) does not require HRPWM. HRPWM capability is most useful for high-frequency PWM requirements of power conversion topologies" , so I guess I am okay with the standard PWM.