This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SM320F28335-EP: Why the DSP board F28335 is not able to compute output when my switching frequency is 10kHz or more?

Part Number: SM320F28335-EP

Tool/software:

While working with DSP F28335 board I have faced issue regarding output computation. 

I was doing Grid connection, for that I have designed PLL(Phase lock loop). My switching frequency for EPWM was 10kHz, simulation time 1/20kHz and DSP clock for EPWM was 200MHz.

While running the hardware I have observed that when my switching frequency is less then 10kHz the output is coming out properly but as soon as I increases the switching frequency beyond 8kHz it is unable to compute the output.

The GPIO pin starts toggling at one-fourth of the simulation frequency and output is not coming out properly.

What could be done to make it work?

I have mentioned the data I have used in my simulation

fsw=10000; %carrier fz
Tinv=1/fsw; %200e-6
Tsim = Tinv*0.5;% 5e-5;%simulation time%100e-6
clk=200e6; %system clk
tbprd=Tinv*clk/2;
GPIO toggling at = 5Khz when EPWM block's are uncommented
GPIO toggling at = 10kHz when EPWM block's ae comment out 
ADC start of conversion is set at EPWM A.EPWM settingsEPWM BLOCKSADC Settings