Other Parts Discussed in Thread: SFRA
Tool/software:
Hello,
I started using TIDM1000 PFC Eval Board with Power Suite tooling.
I went through INCR_BUILDS 1 to 4 but I have an issue with current quality.
My set-up is :
Use of power suite with TI software
TIDM board is supplied with up to 230Vrms (phase-neutral) / 50Hz voltage through an autotransformer (we set the voltage between 0Vrms and 230Vrms)
Earth of TIDM board (connector J3, pin 2) is connected to autotransformer earth
Output neutral of autotransformer is connected to DC mid point for builds 1 to 3 as requested by user manual
500 ohms / 1 kW resistor is used as a load
Im using F28377 µC board, configured as shown here :
Oscilloscope channels :
C1, C2 and C3 : input phase-neutral voltages
C4, C5 and C6 : input phase currents
Test results :
INCR_BUILD_1, input voltage = 120Vrms (phase-neutral), VIENNA_dutyPU_DC = 0.5 :
=> input voltages are noisy because our autotransformer is sized for 230Vrms ; I used 120Vrms to be representative of what is done in user manual
=> nevertheless currents are as expected (fig. 25 and 26 of user manual)
=> I consider this build with my set-up to be OK
INCR_BUILD_2, input voltage = 120Vrms (ph-N), VIENNA_iLRef_pu = 0.2 :
=> currents on phases 1 and 3 (C4 and C6) look correct, while phase 2 current is distorded (C5)
=> I checked PWM signals, they all look correct and are similar together, including for phase 2 (I didn't go into details, I just checked general shape)
INCR_BUILD_2, input voltage = 230Vrms (ph-N), VIENNA_iLRef_pu = 0.11 :
=> input voltages are cleaner now
=> but phase 2 current is still distorded
=> at this step I tested different Kp value for current regulation, without any improvment ; finally I kept default value Kp = 2
INCR_BUILD_3, input voltage = 208Vrms (ph-N), VIENNA_vBusRef_pu = 1.32 [600V] :
=> not in accordance with figure 56 from user manual
INCR_BUILD_4, neutral disconnected, input voltage = 208Vrms (ph-N), VIENNA_vBusRef_pu = 1.32 [600V] :
=> not in accordance with figure 56 from user manual
Do you have any idea why current are distorded ? What can I check ?
I am working with 50Hz input voltages, is it a problem ?
Thanks,
Best regards,
Julien