This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F2800157: GPIO SCI change default value

Part Number: LAUNCHXL-F2800157
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hello,i would like to change the default value of SCIARX/TX ,they are GPIO28/29 by default, and i want to change them to option 2 gpio8/9 in the boot, 

i found the code in C:\ti\c2000\C2000Ware_5_04_00_00\libraries\boot_rom\f280015x\rev1 ,but i dont know how to update it, just manually ? how to flash then the boot , iam alittle b bit lost , thank you in advance

  • Hello,

    By changing the S2 switch you can choose the GPIOs for SCI in LAUNCHXL-F2800157.

    "This LaunchPad allows for one of two sets of pins to be used for the SCIA UART routed to the virtual COM port of the XDS110. By default, GPIO28 (SCIA_RX) and GPIO29 (SCIA_TX) are routed to the virtual COM port and not available on the BoosterPack connector. Alternately, GPIO23 (SCIB_RX) and GPIO40 (SCIB_TX) can be routed to the virtual COM port. When UART functionality is not needed at the virtual COM port, the GPIOs can be routed to the BoosterPack connectors for BoosterPack standard functions."

    Best Regards,

    Masoud